Die Endress+Hauser Gruppe

Medienzentrum

Events

Ihre Karriere bei Endress+Hauser

Unser Support: stets in Ihrer Nähe

Electronic dp improves accuracy, installation & maintenance

New technology solves problems for Lucite International

When the engineers at Lucite International’s Cassel Works in Billingham wanted a better way of measuring the level in a separator vessel, they chose Endress+Hauser’s Deltabar FMD72 electronic differential pressure system. Why? Electronic dp is 10 times more reliable and up to 10 times faster in response times than traditional capillary systems as it is independent of changing ambient conditions.

  • Lucite International’s Cassel Works plant ©LuciteInternational

The benefits

  • Increased reliability

  • Ease of installation due to modular design

  • No need for recommissioning or recalibration

  • Cost-effective

  • Improved speed of response

  • Lucite International ist ein Weltmarktführer für die Konzeption, Entwicklung und Fertigung von Produkten auf Acrylbasis. Seitdem das Unternehmen 2009 von der Mitsubishi Rayon Gruppe übernommen wurde, hat das Unternehmen seine Position als der weltweit größte Lieferant von Methacrylsäuremethylester (MMA), dem Basisbaustein für alle Acryle, noch gestärkt. Lucite International verfügt über eines der breitgefächersten Produktportfolios aller großen Acrylhersteller mit 22 Anlagen an 14 Fertigungsstätten weltweit.

  • Tony Kydonakis at Lucite International
    I chose electronic dp because of its accuracy in measurement and reliability, as well as the benefits of easy installation and maintenance.

    Tony Kydonakis

    I/E Asset Engineer, Lucite International

The challenge

The separator vessel keeps the chemical Bisphenol A (BPA) under vacuum and at high temperature in order to separate off the volatile organics and reuse them, improving yield and plant efficiency. It’s important that the BPA doesn’t enter the downstream process as its viscosity and high sulphuric acid content carries risk of corrosion.

The previous level monitoring system in the vessel was a high level alarm and trip that prevented overfill but gave no pre-warning of any problems. The obvious solution was to install a differential pressure device – mounting sensors at the top and bottom of the vessel in place of existing sight glasses – in order to monitor the level more closely. However, there were concerns over accuracy and speed of response with such solution using oil-filled capillaries.

Installation of a traditional device would also have been difficult as it would have required feeding the capillaries through the floor of the plant in order to mount the transmitters at the top and bottom of the vessel, using the existing tapping points. This would involve maintenance considerations concerning diaphragm seal failure as the process would stop for the duration of the repair incurring significant efficiency losses.

The solution

Unlike other electronic DP systems, Deltabar FMD72 consists of just one transmitter with two sensor modules. Either sensor can be operated as the high or low pressure sensor. Due to the acidity of the BPA in the vessel, the device was supplied with tantalum diaphragm seals to avoid corrosion. Lucite also opted for a HART splitter, which divides the HART signal into two and enables them to measure the vapor pressure at the top of the vessel as an additional parameter.