Information is Key

 

This paper discusses the possibility of using open architectures with flexible structures based on Internet technologies to integrate information from a wide variety of different sources and origins whilst at the same time interacting with on-site plant asset management tools which allow set up, maintenance scheduling, condition monitoring and calibrating of plant assets. 

 

Click here to download (PDF, 966 KB)

 

Integration of sensors into process control and asset management systems

 

Sensors are part of the plant automation network. To achieve the full benefit, they have to be integrated completely into the automation system and information network of a process plant.

 

Click here for download (PDF, 404 KB)

 

ARC Strategies: Need for Business Knowledge Transforms the Role of Field Devices

 

Field device suppliers not only are continuing their investments in sensor technology, they are increasingly expanding beyond traditional thinking into software and diagnostics.

Endress+Hauser's Fieldgate and W@M (Web enabled asset management) are sited as new groundbreaking technologies which aid the transformation.

  

Click here for download (PDF, 266 KB)

 

ARC STRATEGIES: Endress+Hauser - Leading Through Focus & Innovation

 

This report provides a more detailed glimpse of this company, from its initial origins to what it has become today. Through the reading of this report, one will hopefully gain a greater appreciation for a company that has performed admirably over the last fifty years and has certainly put in place a countries culture, an enthusiastic employee base, and a vision that should easily carry it forward for another fifty years.

  

Click here for download (PDF, 1331 KB)

 

Kommentar: Auf die Situation in den USA kommt es an - leider!

 

Dieter Schaudel zum Thema amerikanisches Patentrecht. 

Published in etz

 

Click here for download (PDF, 339 KB)

 

"Wer nicht patentiert, verliert!"

 

Dieter Schaudel zum Thema amerikanisches Patentrecht.

Published in MSR Magazin 9/2003 

 

Click here for download (PDF, 698 KB)

 

Establishing a balanced maintenance strategy for field instrumentation

 

Field instrumentation devices are crucial to reliable process plant operation but often they are not included in the maintenance plan since their reliability is relatively high, but effects of age and technological obsolescence lead to reduced plant performance over time.New legislation demands more control and re-calibration, manufacturers promise very stable and highly reliable instruments. The challenge is now to newly balance the maintenance efforts and their payback.

 

This paper describes a methodology which allows a cost effective approach and improves the important issues such as safety and plant reliability.

Published in atp - Automatisierungstechnische Praxis 44 (2002), Edition 11, P. 38-45

 

Click here for download (PDF, 237 KB)

 

So automate a process automation supplier processes

 

Automation with a future must prove itself in practical application. The Elektrotechnik magazine wanted to know: How does Endress+Hauser (E+H), the process automation supplier, automate processes? The Endress+Hauser plant in Maulburg specialises in the production of numerous variants. Lots of 1 are mastered at that site. (IN GERMAN)

  

Click here for download (PDF, 165 KB)

  

It depends on the right data

 

Nobody has ever controlled or regulated anything that has not been measured beforehand. Automation engineering specialists seem to loose sight of this correct principle because many discussions of recent years have been dominated by "system architecture", "integration", "networking", "open control", "asset management" and other terms and concepts from the realm of informatics. (IN GERMAN)

 

Click here to download (PDF, 765 KB)

  

Against the tide: to the sources

 

Nobody has ever controlled or regulated anything that has not been measured beforehand. This is not a new idea. Neither is it original. And yet, it is often ignored - even by experienced process controllers and, more frequently, by young ones. (IN GERMAN)

 

Click here to download (PDF, 65 KB)

  

Status monitoring and selfcalibration of sensors

 

Precondition for the status monitoring of sensors ist that you have redundant informations. Amongst redundant installation you can use for this fixed known relations between independent signals. Sensor with periodic change of status, resonant systems, general dynamic systems offer a higher security of the status monitoring and selfcalibration you need a comparable exitation corresponding to ther physical measuring quantity. In recent sensors with computing power within the sensor electronics you get supplementary informations about the systems and the reliability of measuring signals in addition to the good / wore status. (IN GERMAN)

 

Click here to download (PDF, 138 KB)