29.11.2011
Endress+Hauser and the Irish National Institute for Bioprocessing Research and Training (NIBRT) have signed a collaboration contract. A tailor-made training facility for biotechnological processes has already been commissioned by Endress+Hauser at the NIBRT in Dublin.
18.11.2011

With its 14-inch diameter and accuracy up to 0.05%, the Promass 83X/84X four-tube Coriolis mass flowmeter is ideal for pipeline custody transfer and other high flow rate applications requiring reliability and low maintenance.

08.11.2011
Proven in more than 3 million applications worldwide, our Liquiphant is the market-leading liquid level switch – and for good reason! Now its application possibilities have opened up further with the introduction of the dual compartment stainless steel housing specially designed for the demands of the oil & gas industry.
24.10.2011
Efficient solar modules with Endress+Hauser flow and level instrumentation.
04.07.2011
Compliance with strict legal requirements, efficient plant management and economical use of resources are essential demands on modern wastewater treatment plants. Online measurement and control of ammonium and nitrate enable plant operators to optimize both energy consumption and discharge quality of their plants. Endress+Hauser offers a compact ion-selective solution that brings these benefits even to small and medium-sized waste water treatment plants (WWTP).
02.06.2011
More than ever before, the economic situation is forcing

companies in all industries to become more cost-conscious

in terms of their production and in particular the energy efficiency.

Visit us at this year's METEC in Düsseldorf and have a look at which perspectives Endress+Hauser can offer to both the the ferrous and non-ferrous metal industry.

26.02.2011
eing successful in the life sciences and biotechnology industries means delivering exactly what customers expect enhanced by added value. At Endress+Hauser we like to believe that this success is contagious and spurs all of us, both ourselves and our customers, to deliver continuously at the highest levels.
03.02.2011
Endress+Hauser opened the European Center of Competence (CoC) dedicated to the life science industry one year ago.
The competence centers are dedicated to the growth and development of sustainable projects and solutions in the life sciences and regulated industries market. This directly corresponds to the strong demand from our customers who have to manage projects according to GAMP.
28.01.2011
The present legislation in terms of water protection and monitoring makes it obligatory for each and every industrial plant to control the quality of their water effluents. This is the case of Senoble in Spain.
01.11.2010
Deltapilot FMB 70 is used to measure level in silos, holding tanks, mixing tanks, filler bowls, balance tanks and other vessels. Watertight CONTITE™ pressure measuring cell and 316L stainless steel housing with polycarbonate sight glass withstand harsh washdown environments.
19.09.2010
We support you in adding years to the lifetime of your plant, while minimizing the risk of unscheduled outages. Let our solutions help you in enhancing the efficiency of the people that run your process. Use the experience of Endress+Hauser in all steps of the revamping process. It pays off, we can prove it.
03.08.2010
The requirements for the waste water plant operator are growing higher up: strict legislative guidelines, economical plant management and more conscientious dealing with resources. Hardly surprising that he is looking for capabilities in order to operate the plant as efficiently as possible.
06.05.2010

More than ever before, the economic situation is forcing

companies in all industries to become more cost-conscious

in terms of their production. Have a look at which cost

reduction solutions Endress+Hauser can propose to both the

primaries as well as the ferrous and non-ferrous metal industry,

particularly in the areas of raw material usage, process optimization

and energy consumption.
26.01.2009

Our customers in all industries are coming more and more under
pressure to measure the cost of their utilities: Water, Air,
Gas (e.g. Natural Gas, other gases or fuels), Electricity and Steam.

It is interesting to confirm that this trend is independent of the
industry. We can see it in small breweries and in big chemical parks.