25.04.2011
Customers' requirements on performance, flexibility and cost efficiency of their analytical measuring systems are ever increasing. The answer to these requirements is the multiparameter controller Liquiline CM442 and its sensor team. With its upgrade and the new sensors based on Memosens technology, customers can now fully rely on one single device for as many as 11 parameters of liquid analysis.
28.01.2011
The present legislation in terms of water protection and monitoring makes it obligatory for each and every industrial plant to control the quality of their water effluents. This is the case of Senoble in Spain.
04.10.2010
Our Liquiline CM442 multi-parameter controller opens completely new dimensions for your measuring point. With sensors for six parameters, Liquiline can be used across a wide range of applications
11.07.2010
With Carbosys CH4, Endress+Hauser offer a system that monitors methane gas emissions according to the Clean Development Mechanism (CDM). It enables companies or even states to balance their overall greenhouse gas emission. Carbosys CH4 is the ideal solution for all factories in emerging countries with highly carbon-loaded wastewater and waste, such as palm oil mills or landfills.
23.04.2010
The stationary Liquistation CSF48 sampler and the portable Liquiport 2010 CSP44 version will revolutionize the world of sampling. They not only comply with all international standards and laws, they also offer a unique level of flexibility for water-related applications. What is even more remarkable - they are the only samplers that can be used as complete measuring stations for six different parameters.
25.03.2010
When it comes to simplicity, the new multiparameter controller from Endress+Hauser sets standards in every respect. Liquiline CM442 and its new sensors make the perfect team to reach the goals set by demanding liquid analysis. Be it in terms of performance, flexibility or cost savings, the new controller meets every requirement. It is the heart of the new analytical platform that is based on Memosens technology and has a central focus on uniformity and ease of use.
15.01.2010
Four out of five Endress+Hauser customers are now opting to use Memosens digital technology when fitting out new plants. With the tried, tested and reliable inductive non-contact transmission of measuring signals and the innovative maintenance concept, Memosens is ideal in all kinds of industries - from life science and chemical industries to water treatment, pulp & paper and energy applications. ...
22.10.2009
It is not a contradiction to say that investments help to reduce costs. Customers of Endress+Hauser have saved up to 50% on their maintenance costs since the commercial launch of Memosens five years ago. Those interested can now calculate the savings to be gained from using the non-contact sensor technology online on Endress+Hauser's web site.
16.10.2009
Endress+Hauser is launching the new TOCII CA72TOC analyzer on the international market in October 2009. The high-temperature analyzer was optimized for industrial wastewater in close cooperation with Aliseca and Bayer Technology Services. Users can rely on its measurements, even in the event of varying pH values and high salt loads.
29.05.2009

The newly developed ORP electrodes Orbipore CPS92 and CPS92D fulfill the special requirements of the pulp and paper and mining industries. They are particularly suitable for heavily soiled media with a high content of suspended solids. Typical application areas are solids, emulsions, dispersions and precipitates. For these applications the electrodes are equipped with an open aperture so that they are not blocked.

29.05.2009

More and More customers require turn-key solutions instead of single instruments. The worldwide trend in water analysis is moving in the direction of tailor-made analytical systems for various online measuring points. Endress+Hauser and Bayer Technology Services (BTS) have teamed to solve these demanding customer projects.