Temperature product news
15.01.2012
A recent trial has proven that Endress+Hauser temperature probes with thermowells made from a new alloy can withstand extreme temperatures up to
1000ºC that are typically found in the furnace of an energy-from-waste facility.
1000ºC that are typically found in the furnace of an energy-from-waste facility.
08.11.2011
Wireless devices are the ideal solution for monitoring important process variables that are uneconomical to measure by conventional methods.
WirelessHART makes it possible to acquire measurements from dense plant areas, remote locations and even moving vessels. What's more, wireless
instruments support advanced asset management solutions, allowing information to be exchanged with the measurement sensor to aid proactive maintenance strategies across an entire plant.
WirelessHART makes it possible to acquire measurements from dense plant areas, remote locations and even moving vessels. What's more, wireless
instruments support advanced asset management solutions, allowing information to be exchanged with the measurement sensor to aid proactive maintenance strategies across an entire plant.
26.09.2011
Temperature transmitter in use - customer EKATO ESD is more than satisfied with temperature measurement and monitoring in the polyethylene production.
23.12.2010
The importance of a temperature measurement converter in thermometers is undoubtedly increasing. Meanwhile a head transmitter is installed in more than 60% of the delivered thermometers. Thereby the requirements on these temperature transmitters are very varied and thus a flexible as well as comprehensive portfolio is necessary. For Endress+Hauser the success story of this transmitter portfolio began 10 years ago.
08.04.2010
Insert with RTD thin film sensor
This thermoresistance insert is designed for universal temperature measurement in any kind of industries. A RTD thin film sensor element which is suitable for temperatures up to 500°C is placed at the tip area of the insert. Due to the innovative internal encapsulation of the sensor an outstanding vibration resistance can be guaranteed. At the other end of the insert a new ceramic terminal block for a reliable and user friendly connection is provided.