Please note:

The versions mentioned in the device list are related to the product versions used by the time of testing.

System compatibility is in the responsibility of the system provider.

In general it is assumed that a possible incompatibility is indicated by an increased first digit, (e.g. PDM V5.2 -> V6.0).

All the kits of device description files that are listed below, can be obtained from the Endress+Hauser Download Area.

 

Unlike previous versions of SIMATIC PDM V6.0 SP1, the "DeviceInstall" software is no longer required. Use the "SIMATIC PDM Manage Device Catalog" tool instead which can be found under "START > SIMATIC > SIMATIC PDM > SIMATIC PDM Manage Device Catalog".

 

The catalog starting with version 6.0 SP1 of SIMATIC PDM is not released for use in any older version of SIMATIC PDM. However, you can use manufacturers' device descriptions which had been created for older versions of PDM.

 

Since Siemens field devices are integrated into SIMATIC PDM, the procedure shown is using the "Levelflex M" from Endress+Hauser as an example.

Integration procedure

  • Extract the device manufacturer's files to any folder: e.g. "C:LevelLevelflex M ". In the case of network drives, ensure that you have linked them via a drive letter.
  • Start the "Manage Device Catalog" tool via "START > SIMATIC> SIMATIC PDM > SIMATIC PDM Manage Device Catalog". Click the "Browse..." button and select the path in which you have saved the files which are extracted in step 1. You are now shown a tree structure depicting all the device installations which are present in this folder and in subordinate folders. Now select which devices you require by marking the corresponding option box. Click "OK" to install the devices.
  • During the installation, the device is automatically copied to the correct folder ("...SiemensPDMSIM_PDMdevicesPASensorLevelEHLevelflex_M"). There are two files in this folder ("HART_Sensor_LEVEL_EH_LevelflexM.dct" and " HART_Sensor_LEVEL_EH_LevelflexM.ddl"). This means that the device is available in the device overview for SIMATIC PDM.

Please note:

  • The "deviceinstall.exe" tool is not supported starting with SIMATIC PDM V6.0 SP1.
  • The Manage Device Catalog" tool doesn't just use files in the selected folder, it also browses all the subfolders in the selected path. If it finds other "*.devices"-type files there, these devices are also made available for installation.
  • Manufacturers' websites offer the possibility of installing device drivers at a later date. Use the search engine to look for these Websites using the search term "SIMATIC PDM".

 

For further information about SIMATIC PDM V6.0 SP1 please go to Siemens Website www.siemens.com