Title

Try searching by key words, order- or product code or serial number e.g. “CM442” or “Technical information”
Enter at least 2 characters to start the search.

More reliability in liquid natural gas trading

Endress+Hauser provided measurement technology for the world’s first liquefied natural gas calibration facility of VSL in the Netherlands

Publication date 05.11.2020

During the transition period between the fossil and renewable energy eras, liquefied natural gas (LNG) is considered a key energy source to realize global emissions targets. LNG is particularly popular as a fuel in the long-distance transportation sector, such as trucks and marine, as it enables compliance with stringent environmental regulations on SOx and NOx emissions in the sector.

In its liquid state, natural gas has a temperature of –163°C and a volume 600 times smaller than its gaseous state, making it efficient to transport. Since, with the usual large transport quantities, even the slightest measurement deviation can make a big difference in billing, accurate mass flow measurements are critically important for reliable trading relationships.

Promass Q serves as reference instrument

However, volume and mass flow measurements carried out at low temperatures are a major challenge for the measurement technology. The golden meters at the new laboratory therefore also include high-precision Coriolis flowmeters from Endress+Hauser, the Promass Q, and novel LNG thermometers. Volume and mass flow can now be determined with a measurement uncertainty of <0.20% and <0.15%, respectively, and lower than 0.08% for density measurements.

Precise temperature measurement

The design of the thermometer developed in cooperation with the experts of the VSL combines the normally contradictory demands for stability against flow-induced vibrations on the one hand and minimization of the heat dissipation error on the other hand.

Gold standard for LNG measurements

The high level of calibration accuracy achieved in the LNG Research & Calibration Laboratory represents a new milestone in the history of flow measurement. Now, for the first time, a measurement uncertainty of 0.5%, which is common for other types of liquid fuels, can also be guaranteed for LNG.

Read more about similar topics:

Downloads

Explore additional resources

document icon
EH_05-11-2020_LNG.zip ZIP, 9.1 MB
download icon Download
Microphone with coffee cup ©Endress+Hauser

Press list

Stay up to date by subscribing to the Endress+Hauser press list.
Endress+Hauser press list

Endress+Hauser regularly sends out press releases on current topics and company information to media professionals.

Select the topics you are interested in:  *
Select the industries you are interested in: *
Personal Data


Fields marked with * are required. You will receive an email with a confirmation of your subscription. The information enlisted is voluntary and your data will only be used for personalizing your newsletters and not be passed onto any third party. For statistical reasons we will perform anonymous link tracking.

Contact us

Find out more from our experts

Martin Raab Head of Public Communication and Group Media Spokesman, global
Kägenstrasse 24153 Reinach BL Switzerland
pictogram email Send email
Tel. (Standard) +41 61 715 7722
Fax +41 61 715 2888