Try searching by key words, order- or product code or serial number e.g. “CM442” or “Technical information”
Enter at least 2 characters to start the search.

Singular excellence

Endress+Hauser has adapted Coriolis technology to be­ viable in single-use applications. The newly developed Proline Promass U 500 measures flow rates with precision and efficiency to match – as well as being ideally built for subsequent recycling.

Proline Promass U 500

Text: Robert Habi
Graphics: 3st kommunikation

Biotech is a rapidly growing market: Using genetically modified cells taken from microorganisms to produce drugs and vaccines is an enabler for new therapies to tackle many serious diseases. The boom in biotech is also changing production techniques. The trend is for smaller batches made using more compact and flexible systems, and increasingly with a continuous process. Absolute purity is a must when working with sensitive cell cultures: “The slightest contamination can ruin an entire batch,” says Samuel Neeser, Coriolis product manager at Endress+Hauser.

In production facilities built around a multi-use design, all components that come into contact with process media need thorough cleaning and sterilization every time. That involves aggressive acids and a lot of energy for generating steam. “Even then, the risk of contamination is still not zero,” says Samuel Neeser. Hence a clear move to single-use technology: Worldwide, one in every two biotech products is now manufactured like this, with every component contacting a medium only once.

Key facts

$38.8 billion

is the projected size of the market for single-use biotechnology in 2030. More aggressive estimates put the figure at over 80 billion US dollars. The 2024 figure already stands at around 18 billion US dollars.

Sophisticated design, high-quality materials

However, this growing segment has so far lacked a precision flow measuring instrument that also meets the strict cGMP standard. Coriolis technology would be ideal here, yet the complex arrangement inside a conventional instrument makes it far too expensive for single use. But that’s changing, with the Proline Promass U 500. The engineers’ trick is to make the instrument out of two separable parts.

Power supply, exciter, sensors and signal processing all go in the base unit. But what the exciter sets in vibration, the measuring tube itself, becomes part of the disposable component. Just like in other high-quality, high-precision instruments, the tube is made of stainless steel; measurement accuracy is to within 0.5 percent. “This separation of the functional units makes Coriolis technology a viable economic proposition in the single-use sector,” says Samuel Neeser. And to ensure that the disposable component does not later end up in the trash, its constituent parts can be separated by material type and then appropriately recycled.

Recycling concept

​​​​The stainless steel measuring tube, once sterilized, is fully recyclable as scrap metal. After steam cleaning, the polycarbonate manifold and the O-rings undergo specialized recycling processes. The packaging film and protective container for the disposable part are recyclable just like everyday household plastics.

Proline Promass U 500 manifold

Manifold: Polycarbonate Makrolon RX1805

Proline Promass U 500 stainless steel measuring tube

Stainless steel measuring tube: Stainless steel 1.4435

Proline Promass U 500 o-rings

O-rings: Silicone VMQ

Plug in and measure

  1. The disposable part of Proline Promass U 500 slides onto the base unit – the sensor part – and is locked in place.
  2. Field calibration is unnecessary as the device automatically verifies the factory calibration data using Heartbeat Technology.
  3. Either mounted to a front panel in skids or as a bench-top version for the laboratory, the flowmeter finds uses at every stage of biopharmaceutical production.
  4. Dosing, adding ultrapure water, filtration – mass flows throughout are determined using the Coriolis measuring principle. The disposable part comes in four nominal widths.
  5. At the end of a production run, the disposable part that contacted the medium is unlocked, removed and disassembled for recycling. The base unit stays in service.

About the product

Promass U 500 is the ideal single-use flowmeter for biopharmaceutical applications in the life sciences industry. It represents the response to the shift from multi-use to single-use devices and from batch to continuous manufacturing. Offering multivariable measurement, Promass U 500 provides enhanced reliability, high accuracy, and industry compliance according to cGMP. The flowmeter is especially suited for up- and downstream applications in the monoclonal antibodies (mAb) process.

Published 20.05.2025

Read more about similar topics:

Downloads

Explore additional resources

document icon
Company magazine 'changes' 1/2025
How the circular economy is gaining momentum
download icon Download

Dive into the world of the process industry through new exciting stories every month with our «changes» newsletter!