drinktec 2017

Process automation – reliable, efficient and from a single source

At drinktec 2017, Endress+Hauser will exhibit measurement technology and automation concepts for all processes using Mixing & Blending and CIP as examples. As global partner, we support the topic of food safety with accredited calibration services, along with self-calibrating and monitoring measurement technology. New device innovations show how you can measure density with high precision and monitor water circuits easily.
Visit us from September 11th to 15th at drinktec in Hall A3 Stand 322.

  • Date
    11.09.2017 - 15.09.2017
  • Offered language
    German

First self-calibrating thermometer – iTHERM TrustSens

100% compliance – 0% effort
Unique sensor technology with self-calibrating function

High process reliability and plant availability through permanent inline self-calibration – the hygienic iTHERM TrustSens thermometer is designed for users in the pharmaceutical, food and beverage industry who require full compliance with FDA and/or GMP rules. iTHERM TrustSens eliminates the risk of non-conformity during production. Coming soon!

More information on TrustSens >>>

Food safety

Product safety is extremely important to food and beverage manufacturers. The ability to clean production plants plays a key role in food safety concepts. We will show you what you need to consider when selecting and installing devices to specifically implement hygiene concepts. Materials that come into contact with process media must also have specific properties. We will explain what these are and which certificates are needed to comply with regulations.

More information on food safety >>>

Heartbeat Technology – on the pulse of the measurement

There is a requirement in the food and beverage industry for measuring tools to be checked quickly and easily to always ensure a reliable and reproducible end product. As part of HACCP concepts and according to the IFS Food 6 Standard, verification and documentation of measuring points at defined intervals is required. For the first time, Heartbeat Technology enables these requirements to be implemented for flow, level and temperature measuring points – while installed, without plant shutdown.

Industry 4.0, digitization, IoT – discover what's behind it

Industry 4.0 is more than just hype. Digitization and the high degree of connective networking in production units increase plant availability and the efficiency of your production facility and thus also guarantees that you can remain competitive in the future. Using comprehensive networking of your work procedures and business methods combined with intelligent, self-monitoring measurement technology, Endress+Hauser implements solutions that revolutionize and simplify production processes.

drinktec 2017

Product highlights